HPCE Thermal Management
Let’s design the Future liquid Cooling together!

Quick connect coupling systems
– efficient components in the area of thermal management
The requirements for quick connect couplings for tempering and thermal management are extremely high. Whether for applications in the area of renewable energies, for computer cooling, in transport or for industrial applications the coupling systems from Parker offer optimally tailored solutions.

Our systems stand out for their high level of compatibility with the broadest range of liquids (for example water or heat exchange oils) and the application environment.

Likewise, their resistance to mechanical stresses is vital. One of the most important requirements in the cooling of electronic systems is the avoidance of any fluid loss, as this is the only way to guarantee fault-free function of the installation.


Our Value added:
  • Wide experience on various thermal management applications
  • A global presence
  • Customer engineering intimacy
  • In-house engineering and manufacturing
Applications

Medical Environments

In medical environments, equipment such as MRI machines, CT scanners, and surgical devices generates significant waste heat during operation. Overheating can lead to malfunctions, compromised performance, and potential damage to sensitive components. Therefore, an effective cooling system is essential to ensure the reliable operation of medical devices.

Given the compact design and high thermal output of these systems, optimized and efficient cooling solutions are crucial. Liquid cooling is particularly advantageous, as it is significantly more effective than air cooling in dissipating heat. We assist our customers in developing comprehensive liquid cooling systems tailored for high-performance medical equipment, ensuring optimal performance, safety, and longevity in critical healthcare applications.

Information Technology

Processors (microprocessors) generate waste heat during operation. This results in overheating of the unit, which can cause malfunction even to the point of destruction of components. A cooling system is then mandatory to guarantee the rapid dissipation of the waste heat. Small dissipation areas and high temperatures demand optimized and highly efficient solutions. As water is 10 times more efficient than air, we provide support to our customers to build complete systems for water cooling for high performance computers, data Centers, microelectronics and telecomunication applications.

Energy Management

Our knowledge in the use of quick connect couplings in the area of solar and wind energy allows the development of bespoke solutions for everything to do with the subject of efficient cooling circuits. For example, intelligent solutions are vital because of the constantly improving performance of the new generation of energy production plants based on high-performance cooling circuits with liquid. Here, our systems are optimally geared to the parameters of pressure, flow and temperature. As the systems are often used in salty sea air, corrosion-resistant materials are essential

Mobile & Transportation

Rapidly increasing flows of goods and further increases in mobility demand extremely reliable and efficient vehicle concepts. Here, the cooling of diesel-powered and electrically driven rail vehicles is highly important, and we provide light weight couplings and connection products adapted to this application. More recently the environmental care drives more and more to the usage of electrical vehicles and ships. Our products are part of the systems built for the liquid cooling of the batteries.

Industrial Applications

From the individual machine to production lines and high-performance lasers, cooling is present in different industries. Quick connect couplings are used in liquid cooling systems both for cooling tools in the production process and for the machine itself. Therefore, Parker provides solutions for liquid cooling and tempering for all types of industries, as semiconductors, laser projectors, plastic industry, electronics (inverters, converters), etc.
Featured Products
Resources

Parker is member of the Open Compute Project (OCP)

Our experts on Thermal Management
Liana Jaskot
Applications & Product Manager
Parker HPCE
Torsten Böhme
Product Support Manager
Parker HPCE
CONTACT US

© Parker Hannifin 2023. | Privacy Policy | Terms & Conditions.
© 2021 Parker Ltd. | Privacy Policy | Terms & Conditions.