Parker engineered a customized rubber-to-metal bonded Integral Seal™ gasket comprised of a rigid aluminum retainer with an edge-bonded, vulcanized fluorocarbon (FKM) sealing element.
The thermal expansion properties of the aluminum matches that of the mating hardware.
The rigid retainer frame serves as a compression limiter to prevent over compression during installation which can cause the sealing element to lose elasticity and sealing force.
A Fuji impression of the new design confirms an even distribution of sealing contact pressure against the mating hardware (in contrast to the incumbent solution).
Using a repeatable metal stamping process we are able to provide consistent bolt hole locations within .008” on our retainers and eliminate misalignment during installation.