Conductive Materials for Electrical Grounding and EMI Shielding
April 17, 2023

Electrical grounding, or earth grounding, is an important aspect of electrical systems not only for safety reasons but also for reducing electrical noise. Electrical noise, sometimes referred to as electromagnetic interference (EMI) or radio-frequency interference (RFI), can negatively impact the performance of electronic circuits, cause errors in measurements of precision sensors, and lead to the malfunction of sensitive electronic devices.

Grounding helps reduce electrical noise in several ways:
1. Providing a reference voltage level: Grounding provides a stable reference voltage level (typically 0V) for all electronic circuits in the system. This common reference point allows for more accurate and consistent signal measurements, mitigating the impact of noise on these signals.

2. Establishing a low-impedance path for noise currents: Grounding creates a low-impedance path for noise currents to flow back to their source or to the earth. By directing noise currents away from sensitive electronic components, grounding helps prevent the coupling of these currents into the circuits and reduces their impact on system performance. This is often done with the use of a conductive gasket or grounding solution. Depending on the design requirements, these gaskets can be conductive elastomers, metallic fingerstock, conductive foams, or conductive fabric-over-foam construction.

3. Shielding: Grounded metallic shields (e.g., in cables or enclosures) can help block the entry or exit of electromagnetic fields that cause electrical noise. When the shield is connected to the ground, it acts as a barrier that absorbs or reflects the electromagnetic radiation, preventing it from interfering with the electronic components inside the shield. Many of the product families developed by Parker Chomerics are designed for EMI shielding and thus meant to serve as a conductive interface between shields and grounded surfaces. These grounded surfaces can be the enclosure itself or ground planes built into printed circuit boards (PCBs). It is important that a shield is grounded, otherwise it will not provide the intended shielding effectiveness.  
Regardless of the specific grounding needs or the reason for grounding solutions, Parker Chomerics has a wide range of grounding solutions for your cost effective, high performance, high reliability, electronic design needs.


In summary, electrical grounding plays a crucial role in reducing electrical noise in electronic systems. By providing a stable reference voltage level, creating a low-impedance path for noise currents, and shielding electronic components, grounding helps maintain the integrity and performance of electronic circuits and devices of all shapes, sizes, and functions.
Ben Nudelman
Global Market Manager
Parker Chomerics 
Electrically Conductive Elastomer Gaskets
Parker Chomerics electrically conductive elastomer gaskets are the superior choice for corrosion resistance, environmental sealing, and cost-effective EMI shielding. Available as molded sheets or parts, allowing for greater part complexity and detail but sometimes at a higher cost; or extruded into strips and either offered as cord stock at length or spliced (fused) to form a continuous seal. Learn More.
PROVEN PERFORMANCE
The leader in Thermally Conductive Interface Materials.
We continue to advance technologies to bring new and enhanced capabilities and efficiencies.

Cooling Innovation for EV Motors with a Zero-Defect Guarantee

Plastic components provide a low-cost, space-saving solution, enabling Original Equipment Manufacturers (OEMs) to meet the integrated cooling requirements of high-torque electric motors. These products are backed by machine-based process monitoring, ensuring each manufacturing and assembly step is completed thoroughly and correctly. 

Solving EV Charging Station Design Challenges: Thermal Interface Materials and EMI Shielding Solutions

Electric vehicle (EV) battery charging stations, also known as EV charging stations or EVSE (Electric Vehicle Supply Equipment), consist of various electronic components and systems that work together to safely and efficiently charge the batteries of electric vehicles. Like most modern, high power electronics, these devices must overcome challenges associate with thermal management and electromagnetic interference (EMI) shielding in order to operate properly and effectively.

Non-Silicone Dispensable Thermal Gel for Automotive Infotainment and Camera Modules

While “electrification” and “EV” buzzwords have taken center stage in conversations about vehicle electronics, drivers of all vehicle types as well as passengers and pedestrians are the beneficiaries of advanced safety, navigation, and entertainment systems.
Electrical grounding products to protect sensitive consumer electronics.
2023 Thermal Interface Material Innovations
Over the last year, Parker Chomerics has developed new, state of the art thermal interface materials, or TIMs, for use across industries and applications. These novel products continue to expand the portfolio of high performance, high reliability thermal gap pads and dispensable thermal gels.
Can't find what you're looking for? Talk to one of our experts.
©Parker Chomerics 2023