THE SOLUTION
Parker Chomerics proposed a custom T-WING heat spreader, approximately 1.5in x 4in, to be directly mounted onto the hot components using a high temperature silicone pressure sensitive adhesive (PSA). Initial test results indicated a 170C drop in case temperature, with no adverse effects to the neighboring components.
The flexibility of the T-WING allowed the firm attachment to multiple chip surfaces with varying heights. Low headroom was not an issue as the overall part thickness was less than 14 mils. This solution proved to be ideal from both a performance and cost standpoint.
CONCLUSION
The Parker Chomerics T-WING solved the hard drive heat problem, a problem exacerbated by a complex set of mechanical constraints, including low headroom, neighboring heat sensitive components, limited airflow, and varying component heights. Designers were impressed by the simplicity, cost, and performance of the T-WING heat spreaders.