CUSTOMER CHALLENGE
Semiconductor image sensors and chips within an automotive camera assembly are prime examples of how increased board densities and higher functioning, smaller form factor components are further necessitating better heat dissipation efforts.
In its design of a multi-function camera vision system, a global manufacturer of automotive camera systems has placed a camera sensor module with a printed circuit board near where there is an embedded chip emitting heat during power cycles.
As the camera lens is in proximity to the PCB, the concern of silicone contamination heightened the specification of the thermal interface material that is necessary to help dissipate the heat.
The thermal material required will have to be non-silicone based and comply with Paint-Wetting Impairment Substances (PWIS) automotive standards. While there are non-silicone thermal gap pads available, due to the high-volume production of the camera assembly, pads were not a feasible option, as only a dispensable thermal material could meet the necessary throughput requirements.