parker.com/chomerics > Case Studies

Case Studies

More coming soon! Sign up to be notified when we post new case studies.

Error-Proofing TIM Application for EV Battery Packs

Thermal  /  Automotive  /  EV
To ensure electric vehicle (EV) batteries operate safely and efficiently, temperatures within the battery electronic control unit must be carefully and proactively managed. THERM-A-GAP PAD 30 Thermally Conductive Gap Filler Pads from Parker Chomerics provide a high-performing solution that fits seamlessly into robotic assembly processes, leading to a faster, more efficient assembly line that remains debris-free. 
EMI Shielding  /  Plastics  /  Automotive  /  EV
Plastic components provide a low-cost, space-saving solution, enabling Original Equipment Manufacturers (OEMs) to meet the integrated cooling requirements of high-torque electric motors. These products are backed by machine-based process monitoring, ensuring each manufacturing and assembly step is completed thoroughly and correctly. 
EMI Shielding  /  Automotive  /  EV
Advanced driver-assistance systems (ADAS) have life-saving capabilities, but electromagnetic interference (EMI) from the high-performing components and diverse design requirements create an engineering challenge. CHO-MUTE™ 9005 and 9025 rise to the occasion, solving these problems with engineering genius by absorbing EMI radiation and ensuring data integrity.
Thermal  /  Automotive  /  Electric Vehicles
Advanced Driver Assistance System (ADAS) modules and infotainment panels have led the way in terms of advancement of electronic systems within passenger vehicles. As cars and trucks continue to modernize, advanced driver options are becoming standard in nearly every class of vehicle. While “electrification” and “EV” buzzwords have taken center stage in conversations about vehicle electronics, drivers of all vehicle types as well as passengers and pedestrians are the beneficiaries of advanced safety, navigation, and entertainment systems. The overarching term sometimes used to summarize these electronics systems is Audio Video Navigation and Telematics or AVNT. 
EMI Shielding  /  Consumer Electronics
A flex circuit cable running through the hinge between a printed circuit board and the display in a laptop computer required an economical shield wrap or tape. The cable acted like an antenna without shielding.
Thermal  /  Automotive  /  Electric Vehicles
A global automotive supplier required a high performing, robotically dispensed, thermal interface material for an automotive ADAS module.
Thermal  /  Automotive  /  Electric Vehicles
A premium automotive infotainment and entertainment system manufacturer required a high performing thermal interface material capable of filling five locations on the PCB, each having different footprints and gap heights.
Thermal  /  Consumer Electronics  /  General Industrial
A leading drone and UAV manufacturer, specializing in a wide range of drone platforms required an EMI shielding and thermal interface material solution to meet EMC regulations as well as improve the performance and reliability of their products.
Thermal  /  Consumer Electronics
Discover how a global manufacturer of smart home devices used a high thermal conductivity thermal gap pad from Parker Chomerics to effectively dissipate heat from both CPU and RAM ICs.
Thermal  /  Telecom
A global IT company who designs and manufacturers on-premises and cloud storage required a customized thermal gap filler pad solution for their next generation of supercomputers.
EMI Shielding  /  Defense
A global manufacturer of 5G telecom base stations required effective thermal management using a high thermal conductivity dispensable thermal interface material to support increased capacity and connectivity for future traffic growth.
Thermal  /  Consumer Electronics
A leading provider of telecommunications equipment needed a cost effective thermal interface material solution to replace gap filler pads on their set-top cable box.
Thermal  /  General Industrial
A leading provider of industrial and commercial LED lighting solutions required a thermal paste or gel that was screen printable, with no pump-out, all while achieving long-term reliability.
Thermal  /  Automotive  /  Electric Vehicles
A global manufacturer of power control modules for EVs needed a fully cured dispensable thermal gel with excellent heat dissipation for their EV DC/DC converter control module.
EMI Shielding  /  Consumer Electronics
Parker Chomerics CHO-SEAL® 1285 electrically conductive elastomer material is a silver-plated aluminum filled silicone EMI shielding gasket, ideal for connectors and I/O switches.
EMI Shielding  /  Consumer Electronics
Parker Chomerics multi-planar z-axis electrically conductive foam EMI gaskets are ideal for applications where foreign object debris (FOD) is a concern.
EMI Shielding  /  Consumer Electronics
Parker Chomerics helped to design in an economical, high performing EMI shielding gasket for a high volume low closure force application.
EMI Shielding  /  Defense
Parker Chomerics helped to design a custom EMI shielded air vent panel, including an electrically conductive elastomer gasket, for a military ground radar cabinet.
EMI Shielding  /  Plastics  /  Consumer Electronics
Parker Chomerics helped an electronics component manufacturer with a total EMI shielding solution shielding components on a PCB. 
Thermal  /  Automotive  /  Electric Vehicles
Discover three challenges a global automotive supplier faced when designing an integrated gauge cluster assembly on an aluminum die cast housing, delivered as a single assembly for instrument cluster module. 
Thermal  /  Automotive  /  Electric Vehicles
Parker Chomerics helped a global manufacturer of automotive electromechanical systems with material knowledge and engineering support to develop an electrically conductive plastic ECU housing for use in an automotive actuator system.
EMI Shielding  /  Life Science
Cables of a life science device needed EMI shielding to improve signal to display monitor.
Thermal  /  Automotive  /  Electric Vehicles
A global automotive supplier required a high performing, non-silicone based and highly conformable thermal interface material for an automotive ADAS camera module.
EMI Shielding  /  Plastics  /  Automotive  /  Electric Vehicles
A global Tier 1 automotive supplier required lightweight alternatives to conventional metal castings for use on a new electric drive unit.
Thermal  /  Telecom
A global manufacturer of 5G telecom base stations required effective thermal management using a high thermal conductivity dispensable thermal interface material to support increased capacity and connectivity for future traffic growth.
Thermal  /  Automotive  /  Electric Vehicles
As the demand increases for electric vehicles (EVs) and hybrid electric vehicles (HEVs) worldwide, manufacturers must also cope with the increase in 12V or 24V accessories that traditionally have been powered by an alternator. In EVs and HEVs, this alternator is replaced with a DC/DC converter which can transfer the energy between the power source and on board accessories.
EMI Shielding  /  IT  /  Consumer Electronics
An electronics component manufacturer requires a filter connector gasket that must be conductive, with z-axis and x-y plane shielding. It must have high reliability on both aging and temperature cycling tests. The customer is currently using a metal gasket with form-in-place (FIP) technology that is not providing the proper performance required.
EMI Shielding  /  Automotive  /  Electric Vehicles
Parker Chomerics helped a global automotive supplier design and assemble a 77 GHz ADAS radar sensor housing with EMI shielding and thermal management materials supplied as a single, fully integrated assembly. 
Thermal  /  IT  /  Consumer Electronics
A global electronics manufacturer was not happy with their current supplier of thermal interface pads. Due to the shear movement of this application, the manufacturer needed a thermal interface gap pad that would not tear under motion.
EMI Shielding  /  IT  /  Consumer Electronics
Discover how one electronics manufacturer used a Parker Chomerics electrically conductive foam gasket to achieve a conductive grommet.
EMI Shielding  /  IT  /  Consumer Electronics
A globally recognized electronics component manufacturer was having service issues with their current supplier. They needed to switch suppliers and find an EMI shielding gasket that offered a low-compression force, high performance all within a cost-efficient material solution that could be easily cut into parts.
EMI Shielding  /  General Industrial
Manufacturer of indoor agriculture equipment needed a vent to cover the dual light bulbs, and some other EMI/RF shielding was required to project the control electronics as well as reduce device emissions. 
EMI Shielding  /  Telecom  /  Defense
A manufacturer of commercial electronics requires vents in two locations on an OEM cabinet enclosure. Both vents required high air-flow and mid-level EMI shielding. A unique requirement for this application was the frame complexity required to properly made with the customer’s chassis.
EMI Shielding  /  Defense  /  Telecom
A manufacturer of mobile military ground radar systems required an air vent that would provide both high air flow and EMI shielding for an electronics enclosure cabinet on a ground vehicle.
EMI Shielding  /  IT  /  Telecom
A component manufacturer required a complete EMI shielding solution for a cover to shield components on a printed circuit board (PCB). This included a conductive cover, shielding gasket, and RF absorbing materials.
EMI Shielding  /  Laminated Solutions  /  Telecom
Discover how one contract computer manufacturer used a Parker Chomerics EMI shielding solution to enhance shielding around a display.
EMI Shielding  /  Plastics  /  Telecom
A global manufacturer of radio communications equipment wished to replace an existing stamped metal housing with a lighter, more effective solution which would allow for access to the device for enhancements and repairs, without soldering.
Thermal  /  Telecom
A desktop computer manufacturer required EMI shielding of expansion ports designed for future upgrade and repair.
EMI Shielding  /  Telecom
An electronics component manufacturer required a shield ground termination for a cable transitioning into a bulkhead. A connector with backshell solution was not appropriate due to the size and cost implications. As with most cable shield grounding applications, a 360 degree peripheral ground was necessary for system EMI compliance.
Thermal  /  Telecom
A computer hard drive manufacturer needs to cool the case temperature of two read/write chips adjacent to one another, to assure over 500k hour MTBF (mean time between failure).
More coming soon! Sign up to be notified when we post new case studies.
We’re constantly innovating in our drive to create the most advanced clean energy solutions.
2023 Thermal Interface Material Innovations
Over the last year, Parker Chomerics has developed new, state of the art thermal interface materials, or TIMs, for use across industries and applications. These novel products continue to expand the portfolio of high performance, high reliability thermal gap pads and dispensable thermal gels.
Can't find what you're looking for? Talk to one of our experts.
©Parker Chomerics 2023