Parker Hannifin

Chemical Processing On-Demand Webinars from Parker EMG
Industrial & Chemical Processing | Webinars

Featured Webinars

In our webinar that is mainly focused on gas leakage, you are going to learn in detail about key influencing factors and what types of seals, sealing systems, materials, and design recommendations Parker Prädifa offers to prevent leakage. These solutions will be illustrated by a variety of application examples across various industries.
Learn about the requirements of hydrogen applications for the sealing systems and the choice of materials and about sealing solutions for hydrogen applications with cryogenic conditions, high pressures and for use in fuel cells and electrolyzers.
In this webinar, learn how Parker Prädifa's modular seal-wiper kit enables the same pneumatic cylinders to be used for a wide variety of applications.
Join our experts The Art & Science of PTFE Fillers. We'll discuss common PTFE fillers, how fillers enhance mechanical and behavioral properties and review case studies.
Learn in our webinar how to find the right sealing solution for your XXL application and master the specific challenges relating to large dimensions. As a specialist in engineered materials, engineering design and process technology Parker Prädifa offers an extensive portfolio of large-size seals and moldings made of polymers such as NBR, EPDM, FKM, PTFE and PEEK, as well as metal.
Our automotive customers continue to face increased restrictions around using high volatile organic compound (VOC) adhesives in their applications. We heard the industry need and have developed a water-based, one-coat adhesive that has nearly zero VOCs and a longer shelf life – with the same level of performance as our solvent-based adhesives. Join Paul Wheeler In Part 1, where you’ll learn how Chemlok 8566 can be used on traditional automotive parts like bushings and suspension systems, rubber track crawlers and mining parts.
Our automotive customers continue to face increased restrictions around using high volatile organic compound (VOC) adhesives in their applications. We heard the industry need and have developed a water-based, one-coat adhesive that has nearly zero VOCs and a longer shelf life – with the same level of performance as our solvent-based adhesives. Join Brady Hultman in Part 2, where you’ll get step-by-step instructions on how to properly prepare your materials and how to apply the one-coat adhesive.
ParCoat® coatings from Parker Prädifa were specifically developed for elastomer products. They prevent mistakes during seal installation, thus ensuring reliable and long-lasting sealing performance. Our webinar will provide you with an overview of the wide variety of ParCoat® coatings, their properties and effects, complemented by examples from the field.
Join our experts The Basics of PTFE:  What is it and how PTFE's physical, mechanical, and behavioral properties make it suitable as a seal material.
Which factors influence the selection of the right seal for your application? In our webinar, you will gain insight into the wide variety of solutions and learn about the key factors influencing the selection of the right seal for your application.
Save money and work safer with Chemlok Cold-Bond adhesives to bond vulcanized rubber-to-metal and rubber-to-rubber at room temperature. Learn how our cold-bond adhesives are VOC-free and are commonly used for belt and conveyor repairs.
This webinar, with typical application examples from diverse industrial sectors, will provide you with a comprehensive overview of sealing solutions for extreme application temperatures, including their suitability for static or dynamic sealing functions.
Chemlok 701 is a newly developed primer for bonding both mainstream castable polyurethanes and tougher to bond high-performance castable urethane products to metal. This primer was designed to perform well in tough environmental conditions like elevated temperatures and high humidity. In addition, the two-component system (CH 701/702) can be used for extreme conditions like direct water exposure at elevated temperatures.
Chemlok 3Stream is a new adhesion additive technology disrupting the LSR industry by transforming regular LSR into self-bonding LSR, without the premium cost and lead time associated with self-bonding LSRs or the labor and volatile organic compounds associated with traditional primer/adhesive applications.
Elastomeric seals provide the necessary barrier between your process and the environment. Leakage can occur when a seal is compromised, leading to unscheduled maintenance and costly downtime. At the worst, leakage can harm personnel or the environment. Identifying and preventing seal failure is critical to minimizing downtime and keeping the environment, health, and safety a top priority.
LORD LokRelease mold release is a family of fast curing release agents designed for use with molded elastomers. This mold release solution provides a semi-permanent, anti-stick surface coating for fast, easy part removal from molds. LokRelease is formulated to increase time between mold-picking and reduce mold fouling in the rubber-to-substrate molding processes. Our mold releases have been used in LORD rubber-to-metal part manufacturing facilities for years.
In this webinar you'll learn the requirements drinking water materials have to meet, how regulations differ in various countries and what solutions Parker Pradifa offers for global use of sealing systems.
It’s tempting to think of vibration isolation as a simple matter of putting a vibration mount between an object and whatever it’s resting on. Anything must be better than no mount at all, right? Actually, it’s not always right. In some cases you can create problems by adding a vibration mount to a system. Learn more about how vibration actually occurs and the basic compromises in implementing vibration isolation.

©Parker Hannifin Corporation | Privacy Policy