Webinar | Universal Sealing Material for Cooling Circuits
Due to the simultaneous presence of polar (coolant/steam) and non-polar (lubricant oil) media, sealing of cooling circuits in diesel engines as well as in hydrogen combustion engines poses a challenge to the sealing materials used that should not be underestimated, i.e., sealing of different media that normally require different types of elastomers with just one sealing material at high temperatures.

So, what can be done if the low-cost standard EPDM material cannot be used because it must be resistant not only against the coolant but also against the lubricant oil? Coolant-resistant FKM materials from Parker Prädifa provide the required broad media resistance at high temperatures
– without sacrificing seal-relevant material properties or media resistance against lubricating oil.

Interested in more content on this topic?
Visit our Trucks & Buses industry page to learn more about the specific products Parker has to offer across many different applications.